请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:BQ79600-Q1 工具/软件:
您好专家
如果 VIO 电压= 0V、BAT (15引脚)电压= 5.5~18V、器件是否可以触发反向唤醒功能、这意味着 INH (16引脚) CAN 输出唤醒信号?
为什么数据表描述使用反向唤醒功能由"12V"供电?

AlexWu
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
工具/软件:
您好专家
如果 VIO 电压= 0V、BAT (15引脚)电压= 5.5~18V、器件是否可以触发反向唤醒功能、这意味着 INH (16引脚) CAN 输出唤醒信号?
为什么数据表描述使用反向唤醒功能由"12V"供电?

AlexWu