请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:UCC25660 工具/软件:
需要创建一个具有以下规格的直流/直流转换器
VIN:-380至410V
Vout:-26到60V
IOUT_max:-26A.
请为我提供相同的低成本解决方案。 谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
工具/软件:
需要创建一个具有以下规格的直流/直流转换器
VIN:-380至410V
Vout:-26到60V
IOUT_max:-26A.
请为我提供相同的低成本解决方案。 谢谢!