请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
零件号:UCC28950工具/软件:
如何在将输出电流保持在 10A 恒定的同时、将输出电压(例如 48V 至 60V)从 390V 更改为 UCC28950?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.