请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:UCC28C40Thread 中讨论的其他器件:UCC28951、 UCC256403、
工具/软件:
直流输入:300V 至 1500V
输出电压:22V DC
输出功率:500W
紧凑和低成本设计。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.