请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:LM5017您好先生
AMP 需要–15V/AMP 200mA 输出
VIN 具有 24V、5V、3.3V、您是否有任何生成–15V 的建议
谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.