Other Parts Discussed in Thread: TPS25810
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号: TPS25810
您好、
Plesae 建议如果我们需要提升 CC1/CC2、我们使用 5V 电压和 10K Ω、这是我们移除此推升设计时的异常情况、谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.