请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:TPS61089 您好,Expert
作为标题,TPS61089在理论上是否可以以此方式使用? 用户外壳为5V 输入,输出为8V 至9V 可调。
谢谢!
落基山脉
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,落基
请参阅以下内容: