This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] LM7481-Q1:VDGATE- VA电压仅为3.6V

Guru**** 1858870 points
Other Parts Discussed in Thread: LM7481
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1092049/lm7481-q1-vdgate--va-voltage-only-3-6v

部件号:LM7481-Q1
在线程:LM7481中讨论的其他部件

你(们)好

我的电路数据报 与规格相同,但VDGATE-VA电压仅为3.6V,  出现此问题的原因是什么

参数如下:

VIN=14V,Vov-GND=0.9V, VCAP-VS-= 12V,VHGATE-VOUT=11V, VEN-GND=5V。

Cin=990uF,Cout=20uF,CVS=0.1uF,CCAP=2.2uF,Q1和Q2使用 FBL8.6062万-F085。

没有D1和D2