请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:BQ2.7542万-G1 您好,
在数据表中,ADC范围为1V,在方框图中,ADC输入通过分用电阻4R和R
这是否意味着ADC可以测量5V,BQ2.7542万可以正常测量4.4V电池?
谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
在数据表中,ADC范围为1V,在方框图中,ADC输入通过分用电阻4R和R
这是否意味着ADC可以测量5V,BQ2.7542万可以正常测量4.4V电池?
谢谢。