Other Parts Discussed in Thread: TLC5945, TLC5944
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:TLC5944 主题中讨论的其他部件:TLC5945,
尊敬的各位:
在数据表中,最大输出电流为70mA。 如果 我将参考电阻器放置在750欧姆参考引脚(输出引脚上的估计电流最大约为65mA),此设备能否处理高达70mA的电流
此致,
马丁
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.