请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:LMR3.363万 LMR3.363万用于在具有50mA负载的3.8V范围内产生3.3V电压。 在切换过程中观察到负电感器电流。
1.此负电流是否会影响模块的稳定性?
2.观察到的负电流的原因是什么。

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
LMR3.363万用于在具有50mA负载的3.8V范围内产生3.3V电压。 在切换过程中观察到负电感器电流。
1.此负电流是否会影响模块的稳定性?
2.观察到的负电流的原因是什么。