您好,TI
当输入电压= 5V时
1.在±4.7V和120mA下是否可以连续输出?
2.压降是否可以小于200mV?
是否有任何产品可以覆盖此芯片,但低温可达-55°推荐?我还需要一款低温版本的终端产品。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,TI
当输入电压= 5V时
1.在±4.7V和120mA下是否可以连续输出?
2.压降是否可以小于200mV?
是否有任何产品可以覆盖此芯片,但低温可达-55°推荐?我还需要一款低温版本的终端产品。
您好,
「盖住这个芯片」是什么意思?
是否要用充油泵替换LM2.7762万? 如果是,我们当前的产品组合中没有任何更新的充电泵。
您是否对降压转换器感兴趣?
此致,
费宾