请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:LM2675 这是LM2675的绝对最大额定值。
我们测量了图中所示电路中CB针脚上的电压,发现该电压比SW针脚高10V。 此结果偏离VSW+8V的绝对最大额定值。
请告诉我如何将升压端子上的电压降低到允许值(VSW+8V),或者升压端子上允许的最大电压是多少。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.