请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:TPS5.4394万 您好,
请告知我们是否可以连接VO1和VO2,输出电流为6A (最大值)? 谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
请告知我们是否可以连接VO1和VO2,输出电流为6A (最大值)? 谢谢。