请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
主题中讨论的其他器件:TLV767我的客户需要一个具有成本效益的 LDO
VINmax 4.2V
输出电压3.3V
输出电流为1.2A
我查看了 TLV767、但它仅为1.0A。
谢谢
Josef
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.