请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS53632 您好!
我对 TPS53632数据表第23页参考应用中使用的功率级 CSD95372A 有疑问。
我们是否可以使用 CSD95378B 并将其 IOUT 与5:1分压器配合使用以进行电流感应? (假设 CSD95378B IOUT=5mV/A;5:1分压器将转换为1mV/A)
谢谢、
Zane
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.