请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:UCC256404 大家好、电源组。
UCC256404数据表的方程式52。 使用分体式电容器配置时、Cr 的公式为所用1/2值的总值。
对于我的设计、每个电容器的分体电容器为22nF。 在下面的等式中输入的是22还是44nF?
此致、
Stuart

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.