Other Parts Discussed in Thread: LM36011
您好的团队:
LM36011、标志寄存器(0x05)、VLED 短路故障置1,芯片是否损坏?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好 Frank:
LM36011、标志寄存器(0x05)、VLED 短路故障 状态:1
2.LED 引脚 ,的电压小于500mV μ V
3.器件 ID 和复位寄存器(0x06) 软件 复位 0 =正常 (默认值) 1 =强制 器件复位
强制 器件复位、标志寄存器(0x05)、VLED 短路故障 为0,然后变为1
7.4.3.2 LED 短路故障
LM36011通过闪存或手电筒模式以及标志寄存器的 VLED 短路故障标志(位[5])进入待机模式
如果 LED 输出出现短路、则设置(0x05)。 如果上的电压、则会发生 LED 短路情况
LED 引脚电压低于500mV (典型值)。 在 LED μs 标志有效前、抗尖峰脉冲时间为256 μ s
通过断开 LM36011的电源或设置软件复位字段(寄存器)、可将 LED 短路故障复位为0
0x06位[7])更改为1、或通过读回 Flags 寄存器来实现。