请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:BQ25611D 1、电流精度小于0.8A 的原因高达6%

2.充电精度为何在+ 5°C 时不能达到6%
(,电流配置为1A μ A 我们预计电流不超过50%(0.5A)@ 5度)
测试结果

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1、电流精度小于0.8A 的原因高达6%

2.充电精度为何在+ 5°C 时不能达到6%
(,电流配置为1A μ A 我们预计电流不超过50%(0.5A)@ 5度)
测试结果