请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:LM5146 主题中讨论的其他器件: LM5145、 LM5143、 LM5117
你(们)好
请推荐合适的产品降压控制器 IC:
A.输入电压:48V
B.输出电流:20A
C.输出电压:0~48V
D.应用:超级电容器充电
e.参考 IC:LM5145或 LM5146
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.