请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:BQ25792 主题中讨论的其他器件: BQ25720、 BQ25730
你(们)好
BQ25792是否可以支持 USB PD 3.0 100W (20V/5A)?
如果不支持、您能否告知哪款器件支持20V/5A 输入以及4S 电池充电电流高达5A?
Edgar
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.