请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS54824 大家好、
您能帮助确认以下问题吗?
请帮助确认是否可以使用1.8VCMOS 电平标准将 TPS54824的 PG 引脚上拉至1.8V?
在以下手册中、仅找到最大6.5V 限值、但似乎没有提到可上拉的电压

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.