请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:BQ25713 各位专家:
关于 BQ25713应用、我有两个问题:
它是否能够使用5mΩ μ A 来实现更高的充电电流、副作用是什么?

2.如果它只用作降压充电器,是否可以移除升压模式 MOSFET Q3和 Q4?

谢谢。
Anderson
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.