Other Parts Discussed in Thread: TPS22916
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS22916 您好!
我们使用的是 TPS22916、我们观察到负载为2.5A 时、输出电压突然下降(3.74V 至2.98V)。
是否有方法可以改善瞬态? 或者是否有其他具有小负载瞬态的负载开关? 谢谢。

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.