请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
主题中讨论的其他器件:LM2594大家早上好、
如果有人这样做、我需要知道通过 TPS2309和 LM2594HVM-12从 POE 电源获得12伏电压是否是个好主意。
对于这两种情况、我都使用参考图。
我已经运行了几个小时的测试、似乎可以正常工作、因为器件将每天24小时运行、我想知道这两个组件的组合是否随着时间的推移而可靠。
谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.