Other Parts Discussed in Thread: TPS51200
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
主题中讨论的其他器件:TPS51200我在数据表中看到 VIN 电压为5V +/-5%。

但网络侧 VIN (最小值) 1.2V。
和(最大值) 3.6V

哪一个是 currect????
请帮您测试 VIN 吗? 如果在输入电压为3.3V 时没有问题、
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.