请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:BQ25601 主题中讨论的其他器件:BQ25606、
您好:
1.充电芯片 bq25601和 bq25606是否可以与 PTP 兼容?
2.如果 bq25601未初始化、bq25601默认可以工作吗? 默认充电电流是多少?
无法连接 bq25601的/QON 引脚。 如果此引脚连接到开关、它是否由手动控制系统供电?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.