TPS7A24数据表的"6.3建议运行条件"中是否描述了"输出电容器"和"输入电容器"?
还是"有效电容"?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
感谢您的回答。
我还有一个问题。
如果"6.3建议运行条件"中"输出电容"的"MAX100uF"为"有效电容"、
是否与"建议有效输出电容值不超过50 μF "不一致。 "8.1.3输入和输出电容器要求"?
"μF μF 输出电容值不超过50 μ F "中的"50 μ F "。 不是"6.3建议运行条件"中"输出电容器"中"MAX100uF"因降额而降低50%的值。 是吗?