主题中讨论的其他器件: TPS61022
尊敬的先生:
我的设计输入5.5V 输出3.9V
如何计算输出电流? 11.9A 2A 或3A?
在 spece2e.ti.com/.../2844.TPS61088.pdf 上 ,输出电压为4.5-12V。 我的设计是3.9V 、 这是正常的吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.