Other Parts Discussed in Thread: TPS51206
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS51206 大家好、
我们在器件中使用 TPS51206。 对于 S3和 S5引脚、由于无法通过 GPIO 进行控制、我们目前正在提供一个直接上拉至3.3V (Vdd)的电源。 请确认这是否正常。
此致、
M Amarnath
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.