请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:BQ76940 大家好、
我在 Bq76940中遇到一个问题,当我连接充电器以40A 电流充电时,第一节电池的电压将提高20-30 mV。
在40A 放电时,第一节电芯电压下降20-30mV,任何克服它的解决方案。
当我断开负载 或充电器时、它会变回正常状态。
谢谢、此致、
Rohit
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.