请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS2384 主题中讨论的其他器件:TPS23882
你(们)好
我的客户需要802.bt 15W 8端口
输入电压为12V 至54V 时、是否有适合产品推荐的任何器件?
谢谢你
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.