请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
主题中讨论的其他器件:TPS7A92、 TPS74901、 TPS7A52、 LP5912您好、E2E、
我们正在寻找 在120Hz 和10kHz @ 5Vin 至3.3Vout 下具有80dB PSRR 的2A LDO。
请提供建议。
~Jason
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.