请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS727 大家好、
我们是否有一个最小负载电流几乎为0的 TI 器件来为客户提供?
其 最小负载应在1uA 至5uA 的范围内。
我们的数据表显示了0mA 负载电流、但在测试 TPS727时、其最小值 约为120uA、以便进行正确调节。
谢谢、
Jonathan
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.