请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:LMR33630 尊敬的:
如何在基准电路中选择电感?以400kHz 工作频率和5V 输出为例、建议电感值为8uH、DCR 和阻抗特性是否有任何特殊要求
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
尊敬的:
如何在基准电路中选择电感?以400kHz 工作频率和5V 输出为例、建议电感值为8uH、DCR 和阻抗特性是否有任何特殊要求