Other Parts Discussed in Thread: UCD7232
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:UCD7232 大家好、
UCD7232是否可用于以恒定电流驱动负载?
我的要求是将珀耳帖元件驱动为最大消耗4A 的负载。
首先、我想驱动3.4的负载。
3.4特定时间段内的最大值、在此之后、我想减小电流、该电流将保持恒定。
谢谢、
此致、
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.