请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:LM3485 LM3485是否有最小负载电流? 我喜欢将 LM3485用于我的应用、因为它具有非常高的负载瞬态响应。 在我的应用中、我将从18V 降至12V、负载将通过 PWM 打开/关闭、因此 负载将从0A 变为2.5A、并快速返回0A。 我还有一个负载完全关闭的情况、我想确保这对于 LM3485不是问题。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.