Other Parts Discussed in Thread: TPS54335A
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS54335A 它是一款输入电压为8至18V 的降压转换器、在我们的 PCB 中输出为5V。 我们系统中的最大电流为1.5A
我们观察到输出引脚(PH、引脚3)短接至 GND。
约10个 TPS54335A IC 发生故障。
4.我们需要您对这一问题的即时支持。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你(们)好
赵的电子邮件 ID 是 zhao-ma@ti.com。
BR
Ruby