请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
主题中讨论的其他器件:LM51551、 UCC28C43您好!
对于部分项目、我需要生成0 (或接近0)至100V、1A (或更低)的可变电压
我有24V 直流电源作为输入
您是否认为可以使用单级直流/直流转换器实现它?
您建议使用哪种 IC 以及采用哪种配置?
谢谢你
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.