请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
主题中讨论的其他器件:TLV767大家好、
我需要选择一个 LDO 双通道:
- VIN<5~6V,Vinmax=9V;
- VOUT 1=3.3V
- VOUT 2=1.8V
解决方案应采用小型封装(例如 QFN 8/14)。
你有什么建议吗?
BR、
Nicolas
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.