请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:UCC28070-Q1 主题中讨论的其他器件:UCC28070、 UCC28180、 UCD3138
尊敬的团队:
我的客户希望使用我们的28070作为升压转换器。 输入为200V、输出为800V、输出功率为35kW-50kW。 请告诉我、如何设计我们的器件以满足客户的要求?
谢谢、此致、
雪利
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.