主题中讨论的其他器件:BQ25713、
大家好、团队、
我已将输入电流感应电阻器从10m Ω 更改为20m Ω、以将 输入电流读数的分辨率从50mA 提高到25mA (ADCIINCMPIN () (2B/2Ah)寄存器)。
对于与输入电流(IIN_HOST (0F/0Eh)和 IIN_DPM (25/24H))相关的其他寄存器、我还需要做哪些其他更改? 我还必须将其 LSB 减半吗?
此致、
Dmitriy
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
大家好、团队、
我已将输入电流感应电阻器从10m Ω 更改为20m Ω、以将 输入电流读数的分辨率从50mA 提高到25mA (ADCIINCMPIN () (2B/2Ah)寄存器)。
对于与输入电流(IIN_HOST (0F/0Eh)和 IIN_DPM (25/24H))相关的其他寄存器、我还需要做哪些其他更改? 我还必须将其 LSB 减半吗?
此致、
Dmitriy
尊敬的林红:
总之、对于20m Ω 的输入电流感应电阻器(RAC):
IIN_DPM 的 LSB (25/24H)是25mA? 寄存器 ofset (0x00的值)是50mA 还是25mA 呢?
2、IIN_HOST (0F/0Eh)的 LSB 是25mA? 寄存器 ofset (0x00的值)是50mA 还是25mA 呢?
ADCIINCMPIN (2B/2Ah)的 LSB 为25mA、全范围为 6.375mA?
此致、
Dmitriy