Other Parts Discussed in Thread: LM25184, LM5180
主题中讨论的其他器件:LM25184、 LM5180
您好!
根据数据表、我确定了3.3输出电压的反馈电阻器。
但是、我在输出端获得的电压超过30伏、并且更改 FB 电阻器没有反应。 变压器1:1
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
尊敬的 Max:
您需要在输出端使用齐纳二极管来钳制无负载电压,例如,对于12V 的标称输出电压为13V。 如果施加一些负载、它应按预期进行调节。
如果匝数比为1:1、则12V 输出的反馈电阻应为121k (例如、请参阅 LM25184 12V EVM)。 此外、初级侧钳位齐纳二极管应设置为反射电压的150%、在本例中为18-24V。 您可以使用 LM5180快速入门计算器来帮助进行组件选择。
此致、
Tim