Other Parts Discussed in Thread: BQ25872
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:BQ25886 您好!
在数据表的第4页上、显示电池充电电压限制可以是8.2、8.4、8.7或8.8。 我很困惑 TI 为什么选择8.7和8.8、因为没有电池化学成分会将电压充电至4.4V、只有锂可充电电池会达到4.3。
谢谢、
Brendan
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.