请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:LMR50410-Q1 主题中讨论的其他器件:LMR50410
大家好、
LMR50410的 Tj 公式目前正在计算中、温度为85℃
1.请帮助确认下标红色框的设置!
Trise & Tfall 是否参考数据表的表7.6? Thx


This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
大家好、
LMR50410的 Tj 公式目前正在计算中、温度为85℃
1.请帮助确认下标红色框的设置!
Trise & Tfall 是否参考数据表的表7.6? Thx


你(们)好
LMR50410具有频率折返特性、这意味着当您具有2.1Mhz 的33V 至3.3V 电压时、基于2.1Mhz 的导通时间将小于60ns、因此器件将保持其最短导通时间工作并调整频率以使占空比稳定。 与最小关断时间相同、当输入电压和输出电压非常接近时、器件将延长导通时间并将关断时间固定在110ns (典型值)、直到其吨数达到7.5us、从而使最大占空比达到大约98%至99%、但此时频率将变为大约133Khz。