请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
主题中讨论的其他器件:PMP8740、 UCC28950、 UCC28951你(们)好
请向我们推荐任何参考设计/IC、以获得0-120VDC、12A 可变电源。
输入电压:230VAC、50Hz
输出电压:0-120VDC、12A
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.