请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS62130A 我们使用 TPS62130A 将电压从2.8V 转换为5V、电路与 TPS62130A_EVM 完全相同、但它在10mF 负载和输出电压下消耗的电流更大、为10.8mA、持续从4.6V 跳转到4.9V、是否有人知道发生了什么?
谢谢、
Feng
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.