请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
主题中讨论的其他器件:TPS2121您好!
我正在为我的电机驱动应用寻找额定电流为2A 的双通道电源选择开关(双输入和单输出)。
我的输入如下
1.电源1 (电池):3V (最大值)和2.5V (最小值)
电源2 (来自 LDO): 3V
让我知道任何额定电流为2A、RDS 极低(Mohms)的选择器开关。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.