请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS54561 大家好 ,我使用 TPS54561,我想得到 Vout =12V,但我发现当负载电流小于4A 时,输出电压随着输入电压的增加而增加,最大输出电压将超过13V (大约 V 输入=50V)。如果 Vout=5V 或 Vout=12,但这里没有负载。将不会发生这种情况 是我的原理图的屏幕截图、能帮我吗?谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.