请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:UC1834-SP 主题中讨论的其他器件:UC1834
你(们)好
UC1834网页上的最大输入电压为36V、 而数据表中的最大绝对值为40V。
很明显 、不能保证 IC 在40V 以上运行、但在36V (<40V)以上运行时会出现什么情况。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.